SBOSAI6 June 2024 THS6232
PRODUCTION DATA
The THS6232 provides output voltage and current capabilities that provide high-voltage and high-current capabilities in a low-cost, monolithic op amp. Under a 100Ω differential load, the output voltage has a typical swing of 21VPP. Under a 25Ω differential load, the output voltage has a typical swing of 16VPP. The THS6232 can also deliver over 310mA of current with a 25Ω load.
If the THS6232 is pushed to the limits of the output drive capabilities, good thermal design of the system is important, including the use of heat sinks and active cooling methods. Figure 6-2, Figure 6-3 and Figure 6-4 show the output drive of the THS6232 under different sets of conditions, where TA is approximately equal to TJ. In practical applications, TJ is often much higher than TA and highly depends on the device configuration, signal parameters, and PCB thermal design. To represent the full output-drive capability of the THS6232, TJ ≅ TA is achieved by pulsing or sweeping the output current for a duration of less than 100ms.
VS = 12V, TJ ≅ TA |
VS = 12V, TJ ≅ TA ≅ 25°C |
VS = 12V, TJ ≅ TA ≅ 25°C |
In Figure 6-2, the output voltages are differentially slammed to the rail and the output current is single-endedly sourced or sunk using a source measure unit (SMU) for less than 100ms. The single-ended output voltage of each output is then measured prior to removing the load current. After removing the load current, the outputs are brought back to midsupply before repeating the measurement for different load currents. This entire process is repeated for each ambient temperature. Under the slammed output voltage condition of Figure 6-2, the output transistors are in the triode region and the transistors start going into linear operation as the output swing is backed off for a given IO.
In Figure 6-3 and Figure 6-4, the inputs are floated and the output voltages are allowed to settle to the midsupply voltage. The load current is then single-endedly swept for sourcing (greater than 0mA) and sinking (less than 0mA) conditions and the single-ended output voltage is measured at each current-forcing condition. The current sweep is completed in approximately 3s to 4s so as not to significantly raise the junction temperature (TJ) of the device from the ambient temperature (TA). The output is not swinging and the output transistors are in linear operation until the current drawn exceeds the device capabilities, at which point the output voltage starts to deviate quickly from the no-load output voltage.
To maintain maximum output stage linearity, output short-circuit protection is not provided. This absence of short-circuit protection is normally not a problem because most applications include a series-matching resistor at the output that limits the internal power dissipation if the output side of this resistor is shorted to ground. However, in most cases, shorting the output pin directly to the adjacent positive power-supply pin permanently damages the amplifier.