SBOU024C august 2004 – july 2023 PGA309
Analog-to-digital converter
Bridge nonlinearity with applied pressure.
Maximum compensable nonlinearity
External feedback capacitor connected between VSJ and VOUT, for stability.
Common-mode rejection
Digital-to-analog converter
Electromagnetic interference
Full-scale range of PGA309 output.
Full-scale bridge sensitivity for sensor at PMAX (for example, 2mV/V).
Ideal gain
Gain of the PGA309 when using the Linearization circuit.
Analog ground
Digital ground
Total gain produced by the PGA309 of VOUT/VIN gain.
GT = (Front-End PGA Gain)(Gain DAC)(Output Amplifier Gain)
Input voltage range of the PGA309.
PGA linearization coefficient
Most negative linearization coefficient. Its value is determined by the selected range of bridge sensor nonlinearity compensation.
Most positive linearization coefficient. Its value is determined by the selected range of bridge sensor nonlinearity compensation.
PGA excitation coefficient. Scale factor on VREF.
Pressure constant. Converts linear input pressure to nonlinear pressure detected by sensor; referenced to full-scale input pressure.
Least significant bit
Most significant bit
Pressure input
Minimum sensor input pressure
Maximum sensor input pressure
Nonlinear pressure output of bridge with linear pressure input P.
Power-on reset function
Single-wire interface program pin
Bridge resistor value
External feedback resistor connected to VFB.
Internal feedback resistor for the Output Amplifier.
Additional external feedback resistor for the Output Amplifier.
Internal gain resistor for the Output Amplifier.
Additional external gain resistor for the Output Amplifier.
External isolation resistor connected to VOUT.
Voltage reference input/output pin
Radio frequency interference
Referred-to-output
Clock input/output for Two-Wire serial interface
Data input/output for Two-Wire serial interface
External temperature signal input
Test/external controller mode pin
Maximum bridge sensor output
Common-mode voltage applied to the PGA309 input.
Coarse offset voltage output of the coarse offset adjust DAC.
Differential voltage applied to the PGA309 inputs.
VDIFF = VINP − VINN
Bridge sensor excitation voltage
Maximum bridge sensor excitation voltage
Minimum bridge sensor excitation voltage
VOUT feedback pin
The output of difference amplifier A3, of the Front-End PGA309.
Signal input voltage 1
Signal input voltage 2
The positive input of internal auto-zero amplifier A1, of the Front-End PGA.
The positive input of internal auto-zero amplifier A2, of the Front-End PGA.
Output voltage of one branch of the bridge.
Output voltage of internal auto-zero amplifier A1.
Output voltage of internal auto-zero amplifier A2.
Sensor offset voltage
Analog output voltage of conditioned sensor
Error in %FSR of VOUT
Filtered VOUT
Ideal output for a given pressure, P.
VOUT for maximum bridge sensor output
VOUT for minimum bridge sensor output
Output voltage of one branch of the bridge.
Reference voltage used by the PGA309 (internal or external).
Temperature VREF
Supply voltage
Analog supply voltage
Digital supply voltage
Output Amplifier summing junction
Test signal
Output voltage of the Zero DAC