SBOU074E january 2009 – july 2023 INA219
To connect the three PCBs of the INA219EVM together, gently push on both sides of the D-SUB connectors (as Figure 3-1 shows). Ensure the two connectors are completely pushed together; loose connections may cause intermittent operation. Finally, connect the SM-USB-DIG to the SENS009 board as Figure 3-1 shows.