SBOU079D july 2009 – july 2023 INA220 , INA220-Q1
Figure 3-3 shows the typical response to connecting the USB DIG platform to a PC USB port for the first time. Note that the EVM must be powered on before connecting the USB cable. Typically, the computer will respond with a Found New Hardware, USB Device pop-up. The pop-up typically changes to Found New Hardware, USB Human Interface Device. This pop-up indicates that the device is ready for use. The USB DIG platform uses the Human Interface Device Drivers that are part of the Microsoft®Windows® operating system.
In some cases, the Windows Add Hardware Wizard will pop up. If this prompt occurs, click Yes to allow the system device manager to install the Human Interface Drivers.