SBOU113A June 2011 – January 2023
To set up the INA226EVM and connect the two PCBs of the EVM together (that is, the INA226 Test Board and SM-USB-DIG Platform board), gently slide the plug and socket ends of the 10-pin connectors together. Make sure that the two connectors are completely pushed together; loose connections may cause intermittent operation.