SBOU113A June 2011 – January 2023
Jumpers J3 and J4 are used to set the hardware setting for the A0 I2C address pin on the INA226. Using J3, the A0 address can be set to either a logic '1' or a logic '0'. Using J4, the A0 address can be set to either the SCL or SDA communication line. Make sure to only have either J3 or J4 connected individually; failure to keep these lines separate can lead to board shorts and problems with the I2C communication lines. See Section 6.2.1 on how to configure the INA226EVM software to match the J3/J4 hardware setting.