SBOU113A June 2011 – January 2023
Jumper J2 selects what connects to the INA226 supply pin. If J2 is set to the INT position, the VS pin is connected to the switchable VDUT signal generated from the SM-USB-DIG Platform. This voltage can be set to either 3.3 V or 5 V, depending on how it is configured in the software. While J4 is set in the INT position, the VS Power button in the INA226EVM software is able to control whether the VDUT supply voltage is turned on or off.
When J2 is set in the EXT position, an external supply connected to terminal T2 can be used to provide the supply voltage for the INA226.