SBOU124B march 2012 – july 2023 INA230
Figure 2-3 shows the block diagram for the SM-USB-DIG Platform. This platform is a general-purpose data acquisition system that is used on other Texas Instruments evaluation modules. The details of the SM-USB-DIG Platform operation are included in a separate document, SBOU098 (available for download at www.ti.com). The block diagram shown in Figure 2-3 gives a brief overview of the platform. The TUSB3210 is the primary control device for the SM-USB-DIG Platform.
The TUSB3210 is an 8052 microcontroller that has an onboard USB interface. The microcontroller receives information from the host computer and interprets the information into power, I2C, SPI, and other digital I/O patterns. During the digital I/O transaction, the microcontroller reads the response of any device connected to the I/O interface. The response from the device is sent back to the PC where the information is interpreted by the host computer.