SBOU124B march 2012 – july 2023 INA230
Users can operate the INA230 software through the Windows Start menu. From Start, select All Programs; then select the INA230EVM program.
Figure 5-1 shows how the software will appear if the INA230EVM is functioning properly.
Figure 5-2 shows an error that pops up if the computer cannot communicate with the EVM. If you receive this error, first check to see that the USB cable is properly connected on both ends. This error can also occur if you connect the USB cable before the SM-USB-DIG Platform power source. Another reason for this error is that there may be an issue with the computer USB Human Interface Device Driver. Make sure that the device is recognized when the USB cable is plugged in; recognition is indicated by a Windows-generated confirmation sound.