This user's guide describes the characteristics, operation, and use of the INA260EVM-PDK (Rev A) hardware. This user's guide discusses how to set up and configure the software and hardware, and reviews the device operation. Throughout this document, the terms evaluation board, evaluation module, EVM PCB, and EVM are synonymous with the INA260EVM. The terms PDK, kit, and EVM kit are synonymous with the INA260EVM-PDK. This user's guide also includes information regarding operating procedures, the input and output connections, an electrical schematic, printed circuit board (PCB) layout drawings, and a parts list for the EVM.
Windows® is a registered trademark of Microsoft Corporation.
All trademarks are the property of their respective owners.
The INA260 is a high- or low-side current sensor, power, and voltage monitor with a 2-mΩ precision integrated shunt resistor and I2C interface. The INA260 offers programmable conversion times and averaging modes that enable high resolution measurements of the current, voltage, and power dissipation of the monitored source.
The INA260EVM-PDK, which consists of the INA260EVM and SM-USB-DIG controller board, is a platform used to evaluate the features and performance of the INA260 under various signal and supply conditions. This document gives a general overview of the INA260EVM-PDK and describes the features and functions to consider when using this evaluation module.