4.1 Quick Start Setup
Follow these procedures to set up and use one of the panels of the INA281EVM. For the following instructions, X is pinout A or B, and n is gain option 1, 2, 3, 4, or 5.
- Choose the desired gain option panel and pin out variation.
- Connect an external dc supply voltage (between 1.7 V and 20 V) to a VS test point, and connect the ground reference of that supply to a GND test point on the same panel.
- Provide a differential input voltage signal to the Vin+ and Vin– nodes by connecting the signal leads to the J1_Xn pin 1 and J1_Xn pin 2 on the EVM, as explained in Section 4.2. The INA281 is a unidirectional current-sensing device because there is no reference pin; therefore, the device can only measure current in one direction.