Follow these procedures to set up and use one of the INA280EVM panels. For these instructions, n is gain option 1, 2, 3, 4, or 5.
- Choose the desired gain option panel variation.
- Connect an external DC supply voltage (between 2.7 V and 20 V) to a VS test point. Connect the ground reference of that supply to a GND test point on the same panel.
- Provide a differential input voltage signal to the Vin+ and Vin– nodes by connecting the signal leads to the J1_n pin 1 and J1_n pin 2 on the EVM, as explained in Section 4.2. The INA280 is a unidirectional current-sensing device because there is no reference pin. The device can only measure current in one direction.