SBOU264B May   2021  – December 2022 INA232 , INA234 , INA236

 

  1.   Abstract
  2. 1Trademarks
  3. 2Overview
    1. 2.1 Kit Contents
    2. 2.2 Related Documentation From Texas Instruments
  4. 3Hardware
    1. 3.1 Features
  5. 4Operation
    1. 4.1 Quick Start Setup
    2. 4.2 EVM Operation
      1. 4.2.1 Setup
        1. 4.2.1.1 Driver Installation
        2. 4.2.1.2 Firmware
          1. 4.2.1.2.1 Firmware Debug
        3. 4.2.1.3 GUI Setup and Connection
          1. 4.2.1.3.1 Initial Setup
          2. 4.2.1.3.2 GUI to EVM Connection
      2. 4.2.2 GUI Operation
        1. 4.2.2.1 Homepage Tab
        2. 4.2.2.2 Configuration Tab
        3. 4.2.2.3 Registers Tab
        4. 4.2.2.4 Results Data Tab
      3. 4.2.3 Current Sensing Operation
        1. 4.2.3.1 Without Shunt Resistor
        2. 4.2.3.2 With Shunt Resistor
      4. 4.2.4 Direct EVM USB Communication
        1. 4.2.4.1 Standard USB CDC Read and Write Operations
        2. 4.2.4.2 Collect Data Through the USB BULK Channel
  6. 5Circuitry
    1. 5.1 Current Sensing IC
    2. 5.2 Input Signal Path
    3. 5.3 Digital Circuitry
      1. 5.3.1 I2C
  7. 6Schematics, PCB Layout, and Bill of Materials
    1. 6.1 Schematics
      1. 6.1.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.1.2 SENS090 (INA232EVM)
    2. 6.2 PCB Layout
      1. 6.2.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.2.2 SENS090 (INA232EVM)
    3. 6.3 Bill of Materials
      1. 6.3.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.3.2 SENS090 (INA232EVM)
  8. 7Revision History
Firmware Debug

If the firmware must be manually reinstalled for any reason, follow these steps to reinstall the firmware. Make sure the EVM is connected to the SCB.

  1. First, see if the GUI can program the firmware manually.
    1. Plug in the SCB controller to the PC.
    2. Launch the GUI.
    3. It is possible that the MCU has already entered DFU mode. If so, the GUI may notify you and try to update the firmware to the latest version.
    4. If it does not update automatically, go to File > Program Device...
  2. If that does not work (or if the Program Device button is grayed out), manually configure the MCU on the SCB Controller to be in Device Firmware Update (DFU) Mode. This can be done through either of the below methods with the SCB Controller powered on:
    1. Through software:
      • For safety, turn off and disconnect all load sources and external voltages.
      • Send the command 'bsl' on the SCB's USB Serial (COM) port.
    2. Though hardware:
      • While shorting the two test points labeled "DFU" (shown in Figure 4-3) with a pair of tweezers (or wire), press and release the RESET button.
        Figure 4-3 Test Points Used to Enter DFU Mode Manually

With the MCU in DFU mode, the firmware can now be uploaded through the method outlined in Step 1.