SBOU264B May 2021 – December 2022 INA232 , INA234 , INA236
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 4-1.
If using multiple EVMs, connect them as shown in Figure 4-2. Make sure to use a different chip address for each device. The GUI only supports one EVM/device type at a time.