Make sure that the previously mentioned
driver was installed successfully to ensure that everything works properly and that the
GUI can update the EVM firmware, if necessary.
Check to make sure the EVM/SCB Controller
unit is plugged into the PC, then go to the previously-provided GUI link.
Click the GUI Composer application
(Figure 4-4) to launch
the GUI from the web browser.
Figure 4-4 GUI Composer Application
Follow the prompts to download the
TI Cloud Agent and browser extension shown in Figure 4-5 for the first-time GUI Composer setup. These prompts will appear after you close
the README.md dialog.
Figure 4-5 TI Cloud Agent
Optionally, click the icon in the GUI
Composer application (Figure 4-4) and follow the
prompts to download the GUI for offline use.