SBOU264B May   2021  – December 2022 INA232 , INA234 , INA236

 

  1.   Abstract
  2. 1Trademarks
  3. 2Overview
    1. 2.1 Kit Contents
    2. 2.2 Related Documentation From Texas Instruments
  4. 3Hardware
    1. 3.1 Features
  5. 4Operation
    1. 4.1 Quick Start Setup
    2. 4.2 EVM Operation
      1. 4.2.1 Setup
        1. 4.2.1.1 Driver Installation
        2. 4.2.1.2 Firmware
          1. 4.2.1.2.1 Firmware Debug
        3. 4.2.1.3 GUI Setup and Connection
          1. 4.2.1.3.1 Initial Setup
          2. 4.2.1.3.2 GUI to EVM Connection
      2. 4.2.2 GUI Operation
        1. 4.2.2.1 Homepage Tab
        2. 4.2.2.2 Configuration Tab
        3. 4.2.2.3 Registers Tab
        4. 4.2.2.4 Results Data Tab
      3. 4.2.3 Current Sensing Operation
        1. 4.2.3.1 Without Shunt Resistor
        2. 4.2.3.2 With Shunt Resistor
      4. 4.2.4 Direct EVM USB Communication
        1. 4.2.4.1 Standard USB CDC Read and Write Operations
        2. 4.2.4.2 Collect Data Through the USB BULK Channel
  6. 5Circuitry
    1. 5.1 Current Sensing IC
    2. 5.2 Input Signal Path
    3. 5.3 Digital Circuitry
      1. 5.3.1 I2C
  7. 6Schematics, PCB Layout, and Bill of Materials
    1. 6.1 Schematics
      1. 6.1.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.1.2 SENS090 (INA232EVM)
    2. 6.2 PCB Layout
      1. 6.2.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.2.2 SENS090 (INA232EVM)
    3. 6.3 Bill of Materials
      1. 6.3.1 SENS079 (INA234EVM, INA236EVM)
      2. 6.3.2 SENS090 (INA232EVM)
  8. 7Revision History
GUI to EVM Connection

To operate the GUI, follow these steps:

  1. Connect to and launch the GUI as described in Section 4.2.1.3.1.
  2. Check to make sure that the EVM connected to the GUI, then close the README.md file page to initiate the connection. If successful, the Hardware Connected message should be visible near the bottom-left corner of the GUI as in Figure 4-6.
    GUID-F8EB79C9-DD17-4A19-BE46-B1EDF62D1C6D-low.png Figure 4-6 Hardware Connected
    1. A green indicator with the device type and the text DEVICE CONNECTED should also be visible near the top-left of the GUI window, as shown in Figure 4-7.
      GUID-20210423-CA0I-0FM1-P28F-MXKC9KR1B5PW-low.gif Figure 4-7 Device Connected
    2. If Hardware Connected and DEVICE CONNECTED do not show in the GUI, check the different hardware COM ports under Options >> Serial Port, as shown in Figure 4-8.
      GUID-E84D10DE-DEAF-4FE9-8D89-9ABCA9B272D8-low.png Figure 4-8 Change Serial Port
    3. If the hardware still does not connect, make sure you are using the correct GUI/EVM combination.
      1. If you are using the correct GUI/EVM combination, you may need to reprogram the firmware of the SCB, as described in Section 4.2.1.2.1.