Figure 2-1 shows an example of how to set up the EVM for dual-supply operation. These steps
can be applied to channel A or channel B of the dual INA.
Figure 2-1 Dual-Supply
Configuration
+VS to test point TP1
–VS to test point TP11
Install jumper shunt to position 1 and 2 on
J1
Differential input signal connect to test points
VinA– (TP14) and VinA+ (TP17) of channel A
Differential input signal
connect to test points VinB– (TP20) and VinB+ (TP22) of channel B
Observe output at test point VOA (TP15)
Observe output at test
point VOB (TP21)
Note: C15 and C22 are prepopulated with 0.1-µF
power-supply decoupling capacitors. See the respective device data sheet for
additional power-supply decoupling information.