SBOU275 April 2022 INA190-EP
R1x 0-Ω resistors that provide the ability to test the device in a "constantly enabled" state. If the EN feature of the EVM does not require discrete control, populate R1x from the panel under test with a 0-Ω resistor prior to powering on the panel to remove this functionality. Ensure that the individual voltages provided to each pin do not violate voltage conditions.