Make sure that the previously mentioned
driver was installed successfully to ensure that everything works properly and that the
GUI can update the EVM firmware, if necessary.
Check to make sure the EVM/SCB Controller
unit is plugged into the PC, then go to the previously-provided GUI link.
Open the GUI Composer application to
launch the GUI from the web browser (see Figure 4-4).
Figure 4-4 GUI Composer Application
The GUI link will bring up all versions
of the GUI. TI recommends to launch the newest version available.
For first-time GUI Composer setup,
follow the prompts to download the TI Cloud Agent and browser extension (see
Figure 4-5). These prompts will
appear after you close the README.md dialog box.
Figure 4-5 TI Cloud Agent
To download the GUI for offline use, click
the icon in the GUI Composer application and follow the prompts (see Figure 4-4).