If the firmware must be manually reinstalled for any reason, follow these steps to reinstall the firmware. Make sure the EVM is connected to the SCB.
- First, see if the GUI can program the firmware manually.
- Plug in the SCB controller to the PC
- Launch the GUI
- It is possible that the MCU has already entered Device Firmware Update (DFU) mode. If so, the GUI may notify you and try to update the firmware to the latest version.
- If it does not update automatically, go to File > Program Device...
- If step 1 is unsuccessful (or if the Program Device button is grayed out), manually configure the MCU on the SCB Controller to be in DFU Mode. This can be done through either of the below methods with the SCB Controller powered on:
- Through software:
- Send the command 'bsl' on the SCB's USB Serial (COM) port.
- Though hardware:
- If the PAMB board is being used instead, these test points are located near PK1 and PK2.
With the MCU in DFU mode, the firmware can now be uploaded through the method outlined in Step 1.