SBOU278 December 2021
This section primarily discusses how to operate the OPT4001EVM software. The GUI has a primary window that is used to configure and read from the OPT4001YMNEVM, along with two other windows that are used to access different features of the OPT4001YMNEVM. Basic GUI functionality and a description of the tabs are also presented in this section.