SBOU285 april 2023 INA700
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 3-1.
If using multiple EVMs, connect them as shown in Figure 3-2. Make sure to use a different address for each device. The GUI only supports one EVM/device type at a time and up to four EVMs total.