SBOU285 april   2023 INA700

 

  1.   SBOU285 Abstract
  2.   Trademarks
  3. 1Overview
    1. 1.1 Kit Contents
    2. 1.2 Related Documentation From Texas Instruments
  4. 2Hardware
    1. 2.1 Features
  5. 3Operation
    1. 3.1 Quick Start Setup
    2. 3.2 EVM Operation
      1. 3.2.1 Setup
        1. 3.2.1.1 Driver Installation
        2. 3.2.1.2 Firmware
          1. 3.2.1.2.1 Firmware Debug
        3. 3.2.1.3 GUI Setup and Connection
          1. 3.2.1.3.1 Initial Setup
          2. 3.2.1.3.2 GUI to EVM Connection
      2. 3.2.2 GUI Operation
        1. 3.2.2.1 Home Tab
        2. 3.2.2.2 Registers Tab
        3. 3.2.2.3 Results Data Tab
      3. 3.2.3 Current Sensing Operation
        1. 3.2.3.1 Detailed Setup
      4. 3.2.4 Direct EVM USB Communication
        1. 3.2.4.1 Standard USB Read and Write Operations
        2. 3.2.4.2 Collect Data Through the USB BULK Channel
  6. 4Circuitry
    1. 4.1 Current Sensing IC
    2. 4.2 Input Signal Path
    3. 4.3 Digital Circuitry
      1. 4.3.1 I2C
  7. 5Schematics, PCB Layout, and Bill of Materials
    1. 5.1 Schematics
      1. 5.1.1 SENS113 (INA700EVM)
    2. 5.2 PCB Layout
      1. 5.2.1 SENS113 (INA700EVM)
    3. 5.3 Bill of Materials
      1. 5.3.1 SENS113 (INA700EVM) BOM
Firmware Debug

If the firmware must be manually reinstalled for any reason, follow these steps to reinstall the firmware. Make sure the EVM is connected to the SCB.

  1. Check to see if the GUI can program the firmware manually.
    1. Plug the SCB controller into the PC
    2. Launch the GUI
    3. Check to see if the MCU entered Device Firmware Update (DFU) mode. If so, the GUI may notify you and try to update the firmware to the latest version.
    4. If the GUI does not update automatically, go to File ➞ Program Device...
  2. If step 1 is unsuccessful (or if the Program Device button is grayed out), manually configure the MCU on the SCB Controller to DFU Mode through the software or hardware:
    1. Through software:
      • Send the command 'bsl' on the SCB's USB Serial (COM) port.
    2. Though hardware:
      • For safety, turn off and disconnect all load sources and external voltages
      • While shorting the two test points labeled DFU (shown in Figure 3-3) with a pair of tweezers (or wire), press and release the RESET button.
        GUID-E745E287-6426-47E8-80F3-99BFA7F04418-low.svgFigure 3-3 Test Points Used to Enter DFU Mode Manually

With the MCU in DFU mode, upload the firmware through the method outlined in step 1.