To connect the GUI to the EVM, follow these steps:
- Set up and launch the GUI as described in Initial Setup
Make sure to connect the EVM to the SCB before powering on
- Close the README.md file page to initiate a connection between the EVM and the GUI. If successful, the Hardware Connected message should be visible near the bottom-left corner of the GUI
- A green indicator with the device type and the text DEVICE CONNECTED should also be visible near the top-left corner of the GUI
- If Hardware Connected and DEVICE CONNECTED do not show in the GUI, long-press the RESET button on the EVM to try again.
- If the long-press reset does not work, check different hardware COM ports under Options ➞ Serial Port, as shown in Figure 3-8.
- If the hardware still does not connect, make sure you are using the correct GUI and EVM combination.
- If you are using the correct GUI and EVM combination, you may need to reprogram the firmware of the SCB described in Firmware Debug.
- Many connectivity issues can be addressed by doing one of the following:
- Long-press the RESET button on the EVM with the EVM and SCB connected to each other.
- Refreshing the GUI may also help
- Connect the EVM to a different USB port
- Avoid using long cables and USB hubs
- If using a desktop PC, try a USB port on the back