SBOU293E November 2022 – August 2024
The OPTEVM software is available through the light sensor IC Product Folder on the TI web site (www.ti.com). The product folder is named corresponding to the specific device part number. To install the software to your computer, navigate to the OPTEVM software. For example, the OPT4001DTS IC is called OPT4001DTSEVM. Open the installer directory. Launch the installation file, for example: OPT4001DTS_EVM_Latte.exe, as shown in the figure below.
The OPTEVM software then begins the installation process, as shown in Figure 4-2.
Follow the prompts as shown in Figure 4-3 to Figure 4-8 to install the OPTEVM software.
The OPTEVM GUI software is now installed.