This section outlines the manual driver
installation process. If the user is using Windows 7 or if the Windows device
manager shows 2 USB Serial Devices under as other devices when the EVM is
plugged in instead of COM ports as shown in Figure 6-1, then use the following steps. If two USB Serial Device devices show up as
COM ports automatically (as is the case with Windows 10), then this section can be
skipped.
- Open the device manager.
- Right click on USB Serial Device and select Properties.
- Click the Update
Driver button.
- Click Browse my computer for driver
software
- Click Let me pick from a list of device drivers on my computer.
- Select Show All Devices and click the
Next button.
- Click the Have Disk
button.
- Click the Browse button.
- Navigate to
“C:\Users\<username>\Documents\Texas
Instruments\Latte\projects\OPT3004\drivers” and choose MSP430_CDC. Click the
Open button.
- Click the OK button
- Select the first USB serial device and click
the Next button.
- Click the Yes button.
- The driver now installs
properly.
- Now repeat this process (steps 1 to 13) for the
second USB Serial Device. All steps are the same except for step 2 and
step 11. In step 2, make sure to right-click the second USB Serial
Device. Likewise, on step 11 make sure to select the second USB Serial
Device when installing the driver as the following figure shows.
- When the driver is
installed, the user sees the following message.
- The two USB Serial Device devices appear in
the device manager under Ports (COM & LPT) as the following image shows.