SBOU293F November   2022  – December 2024

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 OPTEVM Kit Contents
    3. 1.3 Device Information
  6. 2Hardware
    1. 2.1 OPTEVM Hardware Overview
  7. 3Software
    1. 3.1 OPTEVM Software
      1. 3.1.1 Hardware Requirements
      2. 3.1.2 Software Installation
      3. 3.1.3 Typical OPTEVM Hardware Setup
      4. 3.1.4 Launching the OPT300x/4xxxEVM Software
      5. 3.1.5 OPTEVM Software Operation
        1. 3.1.5.1 Getting Started
        2. 3.1.5.2 Feature Descriptions
          1. 3.1.5.2.1 Lux Plot
          2. 3.1.5.2.2 Mean, Std, and the Blue Slider
      6. 3.1.6 Controls
        1. 3.1.6.1 Capture Controls
          1. 3.1.6.1.1 Start Capture and Stop Capture
          2. 3.1.6.1.2 Display Sample Count
          3. 3.1.6.1.3 Save to File
        2. 3.1.6.2 Device Controls
          1. 3.1.6.2.1 Mode Select
          2. 3.1.6.2.2 Conversion Time
        3. 3.1.6.3 Operation Controls
          1. 3.1.6.3.1 Operation Select
          2. 3.1.6.3.2 Measurement/Capture Trigger
          3. 3.1.6.3.3 Oneshot Time (μs)
      7. 3.1.7 OPTxxxDTSEVM Variants
        1. 3.1.7.1 OPT4048DTSEVM
          1. 3.1.7.1.1 OPT4048DTSEVM CIE XY Window
          2. 3.1.7.1.2 OPT4048DTSEVM Lux Live Window
          3. 3.1.7.1.3 OPT4048DTSEVM Channel Live Window
        2. 3.1.7.2 OPT4060DTSEVM
          1. 3.1.7.2.1 OPT4060DTSEVM Channel Live Window
          2. 3.1.7.2.2 OPT4060DTSEVM Lux Live Window
      8. 3.1.8 Scripts Window
        1. 3.1.8.1 Additional Features of the Scripts Window
          1. 3.1.8.1.1 Hidden IDE Window
          2. 3.1.8.1.2 devInit.py
          3. 3.1.8.1.3 04-launchGUI.py
        2. 3.1.8.2 Overview of Device Registers: OPT4xxx Devices
  8. 4Hardware Design Files
    1. 4.1 Coupon Board
      1. 4.1.1 Schematic
      2. 4.1.2 PCB Layout DTS Package
      3. 4.1.3 Bill of Materials (BOM)
    2. 4.2 Motherboard
      1. 4.2.1 Schematic
      2. 4.2.2 PCB Layout
      3. 4.2.3 Bill of Materials
  9. 5Additional Information
    1. 5.1 Trademarks
    2. 5.2 Troubleshooting
      1. 5.2.1 Microsoft Windows 7 Manual Driver Installation
  10. 6Related Documentation from Texas Instruments
  11. 7Revision History

Microsoft Windows 7 Manual Driver Installation

This section outlines the manual driver installation process. If the user is using Windows 7 or if the Windows device manager shows 2 USB Serial Devices under as other devices when the EVM is plugged in instead of COM ports as shown in Figure 5-1, then use the following steps. If two USB Serial Device devices show up as COM ports automatically (as is the case with Windows 10), then this section can be skipped.

OPTEVM OPTEVM on MicrosoftWindows 7 With Drivers not InstalledFigure 5-1 OPTEVM on Microsoft®Windows® 7 With Drivers not Installed
  1. Open the device manager.
    OPTEVM
  2. Right click on USB Serial Device and select Properties.
  3. Click the Update Driver button.
    OPTEVM
  4. Click Browse my computer for driver software
    OPTEVM
  5. Click Let me pick from a list of device drivers on my computer.
    OPTEVM
  6. Select Show All Devices and click the Next button.
    OPTEVM
  7. Click the Have Disk button.
    OPTEVM
  8. Click the Browse button.
    OPTEVM
  9. Navigate to “C:\Users\<username>\Documents\Texas Instruments\Latte\projects\OPT3004\drivers” and choose MSP430_CDC. Click the Open button.
    OPTEVM
  10. Click the OK button
    OPTEVM
  11. Select the first USB serial device and click the Next button.
    OPTEVM
  12. Click the Yes button.
    OPTEVM
  13. The driver now installs properly.
    OPTEVM
  14. Now repeat this process (steps 1 to 13) for the second USB Serial Device. All steps are the same except for step 2 and step 11. In step 2, make sure to right-click the second USB Serial Device. Likewise, on step 11 make sure to select the second USB Serial Device when installing the driver as the following figure shows.
    OPTEVM
  15. When the driver is installed, the user sees the following message.
    OPTEVM
  16. The two USB Serial Device devices appear in the device manager under Ports (COM & LPT) as the following image shows.
    OPTEVM