The Collect Data function reads the desired result registers and sends the data based on the specified settings. This function works best with continuous conversion mode and does not configure the EVM or associated register settings. Collect mode starts and stops via the serial COM port, however the results are sent over the USB BULK channel. To use this mode, use the following format:
- Start collecting data format: collect timerPeriod collectFlags channelAddressIDs numDevices
- Where collect is always lower case, and each parameter is the decimal representation of the value in the following format:
- timerPeriod
- The timer delay used in the MCU to allow data collection sample sets (in µs, unsigned 32-bit value).
- collectFlags (All channels collected together)
- a byte of data that has a 1 to collect and a 0 to not collect each register value type, according to the following definitions (note to only use energy and charge flags when the device supports that, otherwise set to 0):
- VSHUNT = 0b10000
- VBUS = 0b01000
- CURRENT = 0b00100
- POWER = 0b00010
- ENERGY = 0b00001
- channelAddressIDs
- This is the 4 LSBs of each I2C address chained together, starting with bits 3 - 0.
- For example, if EVM 1 is on address 0x41 and EVM 2 is on ox43, the value here is 0b00110001
- NumDevices (Currently only supports a value of 1)
- The number of EVMs chained together (1-4).
- For example, to start data collection for VSHUNT, VBUS, and POWER every 8.8ms, for two INA4235s with EVM 1 address = 0x41 and EVM 2 address = 0x43, the user needs to send: collect 8800 26 49 2
- For this example, the EVM returns the acknowledgment and state in JSON format:
- {"acknowledge":"collect 8800 26 49 2"}
- {"evm_state":"collecting"}
- The USB BULK channel receives data in the format: frameID deviceNumID address registerSize data
- Where each parameter is the decimal representation of the value in the following format:
- frameID (1 byte)
- Always reads 0. Used to verify data is aligned.
- deviceNumID (1 byte)
- An ID number corresponding to the EVM number (currently only supports 1).
- From the above example, this is 1 if reading from EVM 1, which had address set to 0x41, and 2 if reading from EVM 2 which had a address set to 0x43.
- address (1 byte)
- The register address that was read from the device.
- registerSize (1 byte)
- The number of bytes that the following data has.
- data (1 byte at a time)
- The register data value, given in bytes with the most significant byte first.
- Stop collecting data format: stop
- Where stop is always lower case.
- The EVM returns the acknowledgment and state in JSON format:
- {"acknowledge":"stop"}
- {"evm_state":"idle"}