To connect the GUI to the EVM, follow these steps:
- Setup and launch the GUI as described in Initial Setup.
- Check to make sure that the EVM connected to the
GUI, then close the README.md file page to initiate the connection. If
successful, then the text Hardware Connected is visible near the bottom
left corner of the GUI.
- A green indicator with the
device type and the text DEVICE CONNECTED is also be visible near
the top left of the GUI.
- If the text Hardware
Connected and DEVICE CONNECTED do not show in the GUI,
long-press the RESET button on the EVM to try again.
- If that option
does not work, check different hardware COM ports under
Options > Serial Port.
- If the hardware still does
not connect, then make sure the correct GUI/EVM combination is in
use.
- If using the
correct GUI/EVM combination, then reprogram the firmware of the
SCB as described in Firmware Debug.
- Many
connectivity issues can be addressed by doing one of the
following:
- Long-press the RESET button on the EVM with the EVM and
SCB connected to each other.
- Refreshing the GUI can also sometimes help
this.
- Connect
the EVM to a different USB port.
- Avoid using long cables and USB hubs.
- If using a desktop PC, then try a USB port on the
back.