To view and collect results data over time, click
the
(Results Data) icon on the menu to the left. Figure 4-11 shows part of the results data page for reference, which can look different
depending on the connected device.
A description of how to use the buttons and
settings at the top of the results data page and next to each plot is below:
- Results to collect/show:
- Use this section to
select which register values to collect data for. If a results register
is unselected before the COLLECT DATA button is pressed, then the
plot below is hidden and the EVM does not try to read this register
during the collect cycle (even if the conversion is enabled).
- If the user disables one
of these settings while the EVM is collecting data, then the plot does
not show, but data is still collected and the plot updates in the
background. Simply reselect to show data.
- Number of EVMs (GUI support
coming soon):
- Set the Number of
EVMs drop-down menu to the number of EVMs currently in use.
- See Figure 3-2 for how to attach multiple EVMs together.
- Changing this
here also changes the same setting in the Configuration
tab.
- The GUI only supports one
EVM/device type at a time, up to four EVMs total.
- Switch settings
- Use the onboard
switches to select a different address/chip select for each
EVM.
- Set the switch
settings in the GUI to match the setting for each connected
EVM.
- EVM
1 automatically populates with the lowest
addressed device unless a setting has already been
selected.
- Changing
this here also changes the same setting in the
Configuration tab.
- If more than one
device is being used, then a * symbol appears next to the
selected EVM that is being used on the register map and
configuration tabs.
- Changing
the switch settings of any EVM sets that EVM as the
selected EVM.
- Collect and Plots settings:
- Collect Data:
- Press the
COLLECT DATA button to start data collection.
- In this mode, the
MCU reads and sends the selected result values for each device
over a USB BULK channel. All results from one device are read
before moving on to the next device.
- All
result values from all EVMs together are considered one
sample set.
- Currently
all channels are collected per result.
- Although users
can read and write to other registers through the register map
page while collecting data,this can add a delay to the data
being collected.
- Press the STOP
COLLECT button to stop collecting data.
- #Samples Only:
- If this checkbox
is selected, then the GUI automatically stops collecting data
after the number of samples specified in the #Samples box have
been collected.
- If not selected,
then the GUI continues collecting data and only stores the most
recent #Samples.
- Delay between samples:
- Sets the delay
between the start of each sample set.
- Desired delay
time is not obtainable if set faster than the read loop, which
depends on the number of results being collected, the number of
EVMs, and the CPU.
- Although users
can read and write to other registers through the register map
page while collecting data, this can add a delay to the data
being collected.
- Auto Delay:
- Sets delay based
on conversion times, averaging, and number of channels being
converted.
- If multiple EVMs
are being used, then the time put in the delay box is from the
EVM with the shortest calculated delay value.
- Save All Plots:
- Press the SAVE
ALL PLOTS button to save the data for each currently
selected result from the Results to collect/show section
in a spreadsheet.
- Press the SAVE
PLOT button next to each plot to save just the data from
that plot in a spreadsheet.
- Clear All Plots:
- Press the
CLEAR ALL PLOTS button to clear the data from all
plots together.
- Press the
CLEAR PLOT button next to each plot to clear the data
from just that plot.
- #Samples:
- Change the number
in this box to change the number of samples shown in each
plot.
- Changing
this number clears out the plot buffers, so the plots
are cleared on the next read.
- Y-Axis Options:
- Manual Scale:
- Checking
this box sets all channel results in this plot to the
same scale value specified by the Max and Min
fields.
- When this
is not selected, each channel has a Y-axis scale based
on the min and max value for that channel's result
values.
- Max:
- The
maximum Y-axis value to use for all channels in this
plot.
- If this
field is empty when Manual Scale is selected,
then the field auto-populates with the maximum value
currently in the plot.
- Min:
- The
minimum Y-axis value to use for all channels in this
plot.
- If this
field is empty when Manual Scale is selected,
then the field auto-populates with the minimum value
currently in the plot.