To set up the GUI for the first time:
- Make sure that the previously
mentioned driver was installed successfully to verify that everything works
properly and that the GUI can update the EVM firmware, if necessary.
- Check to make sure the EVM/SCB
Controller unit is plugged into the PC, then go to the previously-provided GUI
link.
- Verify that the EVM is
connected to the SCB before plugging the SCB into a USB port.
- Click the GUI Composer
application (see Figure 4-2) to launch the GUI from the web browser.
- The GUI link bring up all
versions of the GUI. TI recommends to launch the newest version
available.
- For first-time GUI Composer
setup, follow the prompts to download the TI Cloud Agent and
browser extension shown in Figure 4-3. Close the README.md dialog box to see these
prompts.
- Optionally, click the
icon in the GUI Composer application (see
Figure 4-2) and follow the prompts to download the GUI for offline
use.