To configure a measurement evaluation, follow these steps:
- Connect a shunt resister by doing
either of the following:
- Solder a 2512 resistor
across the pads of R1 that connects the IN+ and IN– inputs.
- Connect an external shunt
across the IN+ and IN– terminals of J1, preferably across pins 4 and 5,
as shown in Figure 3-3 and Figure 3-4.
- If an external
shunt is being used, then make the connections such that the
sensing location is across the shunt and there is no high
current on the sensing path. See the TI Precision Labs - Current Sense
Amplifiers: Shunt Resistor Layout video for
more information.
- Connect the IN+ and IN– terminals
in series with the load while powered off.
- When measuring more than 10
A, make sure the high current path does not go through the EVM
(including the terminal block J1), as shown in Figure 3-3.
- When using 10 A or less
with either an onboard or external shunt, the current path can be passed
through the EVM. Figure 3-4 shows a convenient way to use the multiple IN+ and IN- terminals with
an external shunt for this use case.
WARNING:
When measuring current, first make sure
that the equipment (shunt resistor, wires, connectors, and so
on) can support the amperage and power dissipation. Secondly,
make sure that the current flowing through J1 does not exceed 10
A. Failure to do so can result in damage to the EVM, or personal
injury.
The EVM can get hot.
- Connect the VBUS terminal (J1 pin
2) to the desired bus voltage (likely either IN+ or IN–).
- If VBUS and dependent
features are not being used, then this channel can be used as an ADC
input for another voltage.
- Connect the system ground to the
GND terminal (J1 pin 1).
- Power on the system, and observe
the device states and outputs through the GUI.