SBVA102 august   2023 TPS56837

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2D-CAP3 Control Architecture
    1. 2.1 Adaptive On-Time Control
    2. 2.2 D-CAP3 Control
  6. 3Large Duty Cycle Operation
    1. 3.1 Min Off-Time Performance of Buck Converters
    2. 3.2 On-Time Extension Function
  7. 4Bench Test and Comparison
    1. 4.1 Comparison Between TPS56837 and TPS56637
    2. 4.2 Comparison of On-Time Extension between TPS56837 and TPS568230
    3. 4.3 Load Transient Improvement by On-Time Extension
  8. 5Summary
  9. 6References
  10. 7Also From TI

Min Off-Time Performance of Buck Converters

The duty cycle increases as the input voltage comes close to the output voltage and the off-time of the high-side switch gets smaller. When the off-time reaches the minimum value, it could not decrease any more, and keeps the minimum value even if the input voltage continues to drop.

Figure 3-1 shows waveforms during normal operation. The on time begins when FB voltage is below internal reference and the off time begins when one-shot pulse comes after a constant on-time timer. The min off-time signal starts the timer once the off-time begins and holds for a constant minimum off-time value shown in the data sheet. If the off-time is longer than the min off-time, the signal won't works.

GUID-20230822-SS0I-CCZR-DH42-VHGKMZ19HMMB-low.svgFigure 3-1 Normal Operation without Min off-time Triggered
GUID-20230822-SS0I-QR4V-KWMK-XRXCVS5TP704-low.svgFigure 3-2 Operation with Min off-time Triggered

Figure 3-2 indicates the operation of converter when the min off-time is triggered. After the off-time decided by the loop is shorter than minimum off-time, even though the FB voltage is less than reference voltage, the off-time no longer follows the VFB comparator but just operates the constant min value while the on-time is still decided by the one-shot circuit and proportional to the VOUT/VIN. With such two limitation, the output voltage would finally fall under the rated reference value and reaches another balance.

Without on-time extension function, it is obvious that the duty cycle is fixed when min off-time is triggered. Based on Equation 3, since Toff has a minimum value, it follows that the duty cycle, D, has a maximum value. If the FSW is fixed, a smaller TOFF(min), means a larger duty cycle can be supported. Alternatively, if the TOFF(min) is fixed, a larger duty cycle can be supported with a smaller FSW.

Equation 3. GUID-7D961473-EFD9-4697-BD86-4B41A54230F7-low.gif