SBVA102 august   2023 TPS56837

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2D-CAP3 Control Architecture
    1. 2.1 Adaptive On-Time Control
    2. 2.2 D-CAP3 Control
  6. 3Large Duty Cycle Operation
    1. 3.1 Min Off-Time Performance of Buck Converters
    2. 3.2 On-Time Extension Function
  7. 4Bench Test and Comparison
    1. 4.1 Comparison Between TPS56837 and TPS56637
    2. 4.2 Comparison of On-Time Extension between TPS56837 and TPS568230
    3. 4.3 Load Transient Improvement by On-Time Extension
  8. 5Summary
  9. 6References
  10. 7Also From TI

Comparison of On-Time Extension between TPS56837 and TPS568230

Both TPS568230 and TPS56837 have On-time Extension function, but their implement is different.

The OTE of TPS568230 is decided by its duty cycle. When the 1.2 < VIN/VOUT ≤ 1.6, the TON will be extended one time interval. When the VIN/VOUT ≤ 1.2, the TON will be extended two time intervals. Thus it would lead to a sudden change of frequency during OTE operation.

The OTE of TPS56837 can slow down its frequency smoothly during OTE operation, which lead to a better performance during OTE operation.

Figure 4-7 provides a frequency changes with duty cycle of both TPS568230 and TPS56837.

GUID-20230824-SS0I-XKLH-L6N4-FMF01PTMLS0Q-low.svg Figure 4-7 Frequency Changes with Duty Cycle

For TPS568230, due to the on-time and frequency sudden change, the output voltage would have a transient process at the boundary of its OTE condition. On the other hand, during OTE process, the frequency of TPS56837 would change smoothly and have a better line transient performance.

Figure 4-8 and Figure 4-9 shows the line transient performance under large duty condition. Obviously we can see TPS568230 has about 12mV voltage overshoot at the two boundaries while TPS56837 doesn't.

GUID-20230820-SS0I-TGFC-RRK6-3N9RMNQS3BWZ-low.svgFigure 4-8 Line Transient of TPS568230 (VIN from 8 V to 6 V)
GUID-20230820-SS0I-957N-FX4V-W309KKQWWPCH-low.svgFigure 4-9 Line Transient of TPS56837 (VIN from 8 V to 6 V)