SBVS343A March 2019 – September 2019 TPS7A78
PRODUCTION DATA.
The TPS7A78 uses a switched-capacitor charge pump to reduce the rectified DC voltage at the SCIN pin by four times, providing the LDO block with an input voltage above its dropout voltage that is then regulated to the target output voltage. The DC voltage at the SCIN pin can be provided either by the active clamp for the bridge rectifying the input VAC supply or by a direct DC supply connection to the SCIN pin.