SBVS360A February 2020 – November 2020 TPS7B85-Q1
PRODUCTION DATA
The power-good delay period is a function of the external capacitor on the DELAY pin. The adjustable delay configures the amount of time required before the PG pin becomes high. This delay is configured by connecting an external capacitor from this pin to GND. Figure 7-3 illustrates the typical timing diagram for the power-good delay pin. If the DELAY pin is left floating, the power-good delay is t(DLY_FIX). For more information on how to program the PG delay, see the Section 8.1.8.2 section.