SBVS393B December 2020 – November 2022 TPS7A43
PRODUCTION DATA
The adjustable-version device requires external feedback divider resistors to set the output voltage. VOUT is set using the feedback divider resistors, R1 and R2, according to the following equation:
To ignore the FB pin current error term in the VOUT equation, set the feedback divider current to 100 times the FB pin current listed in the Section 6.5 table. This setting provides the maximum feedback divider series resistance, as shown in the following equation: