SBVS453 May 2024 TLV770
PRODUCTION DATA
The device has an internal current limit circuit that protects the device during overcurrent or shorting conditions. The current-limit circuit, as shown in Figure 6-1, is a brick-wall scheme. When the device is in current limit, the device sources the output current limit (ICL) and the output voltage is unregulated. In this scenario, the output voltage depends on the load impedance.
During a current-limit event, the potential for high power dissipation exists because of the elevated current level and increased input-to-output differential voltage (VIN – VOUT). If the device heats enough, the device enters thermal shutdown. If the current-limit condition is not removed when the device turns back on after cooling, the device reenters thermal shutdown. This cycle continues until the current-limit condition is removed. The device survives this fault, but repeatedly operating in this mode degrades long-term reliability.