The operational area of an LDO is limited by the
dropout voltage, output current, junction temperature, and input voltage. The
recommended area for continuous operation for a linear regulator is given in Figure 7-3 and is separated
into the following parts:
- Dropout voltage limits the minimum differential voltage between the input and the output (VIN – VOUT) at a given output current level. See the Dropout Operation section for more details.
- The rated output current limits the maximum recommended output current level. Exceeding this rating causes the device to fall out of specification.
- The rated junction temperature limits the maximum junction temperature of the device. Exceeding this rating causes the device to fall out of specification and reduces long-term reliability.
- The shape of the slope is given by Equation 4.
The slope is nonlinear because the maximum-rated junction
temperature of the LDO is controlled by the power dissipation across
the LDO. Thus, when VIN – VOUT increases the
output current decreases.
- The rated input voltage range governs both the minimum and maximum of VIN – VOUT.
Figure 7-3 shows the
recommended area of operation for this device on a JEDEC-standard high-K board with
a RθJA, as given in the Thermal Information
table.