SBVS457A August 2024 – September 2024 TPS7A20U
PRODUCTION DATA
If the input voltage is lower than the nominal output voltage plus the specified dropout voltage, the device operates in dropout mode. In this mode, the output voltage tracks the input voltage. In this mode, the transient performance of the device becomes significantly degraded. During this mode, the pass transistor is driven fully on. Line or load transients in dropout potentially result in large output voltage deviations.
When the device is in a steady dropout state, the pass transistor is driven fully on. This state is defined as when the device is in dropout, directly after being in a normal regulation state, but not during start-up. Dropout occurs when VIN < VOUT(NOM) + VDO. When the regulator exits dropout, the input voltage returns to a value ≥VOUT(NOM) + VDO. During this time, the output voltage potentially overshoots for a short period of time. VOUT(NOM) is the nominal output voltage and VDO is the dropout voltage. During dropout exit, the device pulls the pass transistor back from being driven fully on.