Use the following steps when connecting the equipment:
- Set the input and bias power supplies to 6.5 V (maximum), and turn the power supplies off.
- Connect the positive voltage lead from the input power supply to VIN at the J1 or J2 connector of the EVM.
- Connect the ground lead from the input power supply to GND at the J8 connector of the EVM.
- Connect a 0-A to 3-A load between OUT and GND.
The connector used depends on the desired output current.
- Disable the output by floating J3.