Figure 3-2 shows a HB connection diagram.
To verify proper connectivity:
- Set the AC input power supply
to 120 VAC and 60 Hz, and turn the power supply off.
- Connect the line lead from the
AC power supply to the line pin on the J2 connector of the EVM.
- Connect the neutral lead from
the AC power supply to the neutral pin on the J10 connector of the EVM.
- Connect a 0-mA to 30-mA load
between J3 connecter, to LDO_OUT, and J11 connector, to GND, of the
EVM.