SBVU073A november 2021 – june 2023 TPS7A14
EN is a 3-pin header used to enable or disable the TPS7A14.
The center pin of the 3-pin header is tied to the TPS7A14 EN input. When the 2-pin shunt is placed across the top two pins of the header, VIN is shorted to EN, and the TPS7A14 is enabled. When the 2-pin shunt is placed across the bottom two pins of the header, GND is shorted to EN, and the TPS7A14 is disabled.
When driving the EN terminal with an off-board supply or signal generator, the applied voltage must be kept between 0 V and 5.5 V.