LeCroy is a trademark of Teledyne LeCroy.
Kapton is a registered trademark of DuPont.
All trademarks are the property of their respective owners.
The Texas Instruments' TPS7A13EVM-057 evaluation module (EVM) helps designers evaluate the operation and performance of the TPS7A13 LDO voltage regulator. As shown in Table 2-1, the TPS7A13EVM-057 contains one TPS7A13 LDO voltage regulator in the DSBGA package. An optional load transient circuit is also included to assist the user with high-speed load transient testing. An input current loop is included that allows fast measurements of the input current.
EVM ORDERABLE NUMBER | VOUT | PART NAME | PACKAGE |
---|---|---|---|
TPS7A13EVM-057 | 0.9 V | TPS7A1309PYCKR | 6-pin DSBGA |
This section describes the jumpers and connectors on the EVM, and how to properly connect, set up, and use the TPS7A13EVM-057. Section 3.1 and Section 3.3 describe the test setup and operation for the TPS7A13 LDO. Section 3.2 and Section 3.4 describe the test setup and operation of the optional load transient circuit.