SCDA050 July   2024 TMUX9832 , TX7516

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Front-End Architecture Comparison
  6. 3Routing Topologies for Transmitters With Multiplexer Switches
  7. 4Layout Example – Interwoven Input With TMUX9832 BGA Package
  8. 5Extending the Architecture to Implement Higher Channel Count Systems
  9. 6Summary
  10. 7References

Routing Topologies for Transmitters With Multiplexer Switches

Broadly, there are two ways to organize the connections between the transmitters and the mux switches. This section shows an example system with two 16CH transmitters and two 32CH multiplexers, but the concepts and routing topologies outlined here can be extended and applied more broadly.

The first is an interwoven input style (Figure 3-1), referring to how the multiplexer switch inputs are routed. Each adjacent switch input connects to sequential transmitter outputs. The transmitter outputs repeated to connect the additional multiplexer IC and hence interweaving with connections to the previous. The advantage is that on the output side, the routing from the multiplexer to the transducer is optimized for orderly connections. Additionally, only one clock cycle is required to update the state of all switch channels during scan, resulting in a faster system switching time.

The second is an interwoven output style (Figure 3-2) referring to how the multiplexer switch outputs are routed. Each adjacent switch output connects to disparate transducer elements and interweave as a result. The advantage is that on the input side, the routing from the transmitter to the multiplexer is optimized for short connections between switches. Additionally, because only half of the channels on each multiplexer can be active at a time, power dissipation is divided evenly between each IC.

 Interwoven Input Routing
                    Topology for 64-CH Ultrasound Front End Figure 3-1 Interwoven Input Routing Topology for 64-CH Ultrasound Front End
 Interwoven Output Routing
                    Topology for 64 CH Ultrasound Front End Figure 3-2 Interwoven Output Routing Topology for 64 CH Ultrasound Front End

Table 3-1 compares the tradeoffs between the interwoven input and interwoven output routing approaches.

Table 3-1 Tradeoff Comparison Between Interwoven Input and Interwoven Output Routing Styles
Topology (64-CH ) Interwoven Input Interwoven output
Benefits
  • Optimized routing between multiplexer and transducer. Output pins are ordered the same as piezo elements
  • Only one clock cycle required to update the state of all switch channels during scan (faster system switching time)
  • Depending on system use case, SET/CLR can be used to turn all channels ON/OFF with 1 GPIO only and remove need for SPI
  • Optimized routing between transmitter and multiplexer. Each transmitter channel goes to one IC. Input pins on mux are adjacent to each other and can be shorted at the IC
  • Half of the channels are used at a time and power is dissipated between the two muxes
Limitations
  • Interweaving routing required between transmitter and mux pins
  • Possible for all 32CH of the mux to be excited simultaneously and dissipate higher power per IC
  • Interweaving routing required between mux output pins and piezo elements