SCDS420E September 2020 – July 2024 TMUX6219
PRODUCTION DATA
Break-before-make delay is a safety feature that prevents two inputs from connecting when the device is switching. The output first breaks from the on-state switch before making the connection with the next on-state switch. The time delay between the break and the make is known as break-before-make delay. Figure 6-6 shows the setup used to measure break-before-make delay, denoted by the symbol tOPEN(BBM).