SCDS423A October 2020 – May 2024 TMUX1575
PRODUCTION DATA
Source leakage current is defined as the leakage current flowing into or out of the source pin when the switch is off. This current is denoted by the symbol IS (OFF).
Drain leakage current is defined as the leakage current flowing into or out of the drain pin when the switch is off. This current is denoted by the symbol ID (OFF).
The setup used to measure both off-leakage currents is shown in Figure 6-2.