SCDS429G February 2021 – July 2024 TMUX7234
PRODUCTION DATA
There are two types of leakage currents associated with a switch during the off state:
Source leakage current is defined as the leakage current flowing into or out of the source pin when the switch is off. This current is denoted by the symbol IS(OFF).
Drain leakage current is defined as the leakage current flowing into or out of the drain pin when the switch is off. This current is denoted by the symbol ID(OFF).
Figure 6-2 shows the setup used to measure both off-leakage currents.