SCDU039 May 2024
The TMUXS7614DEVM requires a single supply (4.5V to 42V), dual supplies (±4.5V to ±25V), or asymmetric supplies (such as VDD = 37.5V, VSS = –12V) provided either through the J3/J2 terminals or J14 terminal. The VDD supply can also be provided directly to the VDD test point in the center of the board. The green LED acts as a power indicator for the digital supply VL. On revision 1 boards, this LED can only be powered by the 3.3V supply from the USB2ANY. On revision 2 boards, the LED can be powered by either the USB2ANY interface or an external source via the EXT_VL path.
Do not leave EVM powered when unattended. |