The Home tab is
displayed when launching the hardware software. Make sure the USB2ANY is
connected to the computer and connected with the notch down to the EVM
before using the GUI. If there is a successful connection, then
Hardware connected is shown at the bottom left corner of the
GUI.
The Home tab includes the
SPI signal controls using eight toggle switches to control each channel
individually. To send a SPI signal to close or open the switches, click
on the toggle switch to turn on or off the channels.
Address mode turns on
automatically when a switch is toggled. This mode can also turn on when
the checkbox for Address mode is selected. Please note, when enabling
Address mode by clicking on the checkbox, the first switch closes.
The Home tab also
shows the error detection flags and features for the GUI, but are
currently not operational and will be implemented in a future
revision.
From the Home tab,
the user can go into Daisy Chain and Registers tabs. The
Info, Setup, and Data tabs are currently not
operational and will be implemented in a future revision.
Figure 3-2 TMUXS7614D-SPI-EVM GUI
Home Tab
Daisy Chain Mode Tab
Daisy Chain Mode
tab can be accessed from the Home tab, by clicking on the
Daisy Chain Mode button.
When opening the Daisy
Chain Mode tab, the button is displayed, and when
pressed, sends a 0x2500 signal to enable daisy chain mode.
The select bar can select
a number of devices to control on the daisy chain.
To send signals to the
devices on the daisy chain, click on the checkboxes correlated to the
switch of the device.